Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 11 crashed with java exit code 805306369

Experimenter
Experimenter

Hello everybody,

 

I've just discovered this forum for NX + TC. And, that's my first post. I'm sorry, I don't know if there is a special area to post teamcenter question.

 

So, I will try to explain as best as possible my problem.

 

Yesterday, in my big company, we installed TC 11 and NX 10. (I don't know if there is a link with my problem).

it worked well yesterday.

I've java rev 7.60.

 

This morning, When I want to explore a folder in TC, it's loading... but never succeed.

When it works, only 1minut, I can have access to a part in TC, but when I click to open the pdf, or the 3d file, TC crashed.

 

Can someone help me ?

 

Thanks a lot.

 

Best regards.

 

Nicolas.

 

9 REPLIES 9

Re: Teamcenter 11 crashed with java exit code 805306369

Siemens Genius Siemens Genius
Siemens Genius

Hi Nicolas,

 

To me, it looks like the Java version issue.

 

For Hardware & Software Certifications, please check here:

http://www.plm.automation.siemens.com/de_de/support/gtac/certifications.shtml#lightview-close

Re: Teamcenter 11 crashed with java exit code 805306369

Experimenter
Experimenter

Hi,

 

I don't touch anything this morning and it's ok.

Thanks for your help

 

BR

 

Nicolas

Re: Teamcenter 11 crashed with java exit code 805306369

Phenom
Phenom

Could be a memory issue with Java.

 

Increasing MaxPermSize in TC_ROOT\portal\Teamcenter.ini might help.

 

MaxPermSize=128m

Re: Teamcenter 11 crashed with java exit code 805306369

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I did notice that you're using different values for Xmx and Xms, make them identical. Btw, 2024 is really big. You might want to dial to back to 1024 or even 512.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11 crashed with java exit code 805306369

Legend
Legend

I had similar problem with TC11.2.1 & JRE1.8U31. PFA snapshot. Restarting TC fixes the problem but we need some solid fix. Any recommendations ?

Re: Teamcenter 11 crashed with java exit code 805306369

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
One thing that sticks out is the difference in paths for Java and Portal. Windows isn't case sensitive but Java is so even small things like the below can cause issues:
C:\Siemen\TC11
C:\SIEMENS\Java

Which is it? Siemens or SIEMENS. Might not be the issue but worth looking into.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11 crashed with java exit code 805306369

Legend
Legend

Thanks Randy. I do get java error occasionally.

 

It is SIEMENS. Java.png

 

Re: Teamcenter 11 crashed with java exit code 805306369

Hi!

 

We have the same problem with Teamcenter!

Teamcenter is slow and crash.

 

Anyone who solved this problem?

Re: Teamcenter 11 crashed with java exit code 805306369

Legend
Legend

I created an IR for this intermittent java crash.

GTAC confirmed that they have internal PR filed on it and it is expected to fix in 11.2.3 early December 2016.