Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

I have Visual Studio in two different flavours, 2010 and 2015.

 

Which one would you use under Teamcenter 11? (ITK)

 

I would like to use VS2015 as its IDE colours are much more motivating, still missing the Clip, the Wizard , the Dog and Einstein that made Office so amazing in 1997. Computers and life in general are becoming increasingly boring since then.

 

Should I stay in VS2010 or should I go? 

 

descarga (1).jpg

7 REPLIES 7

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

We always use certified versions,

for Teamcenter 11: 

MSVisual Studio 2012 Update 1 Standard & Professional Edition with hotfix KB2781514

 

see there:

https://www.plm.automation.siemens.com/en_us/support/gtac/certifications.shtml#lightview-close

 

best regards

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

Thank you for your quick answer :)

Highlighted

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

 

But I am only allowed to choose between two flavours... 2010 or 2015, nothing in between. Some changes were made in VS2012 that affected inline functions for std and that is what scares me as I do not know if TC11 libraries were compiled in the old format or not.

 

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

Ok, I don't know how the TC 11 libraries are compiled (old format or not)

maybe somebody else can help here

 

BR

 

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
@PLMFan, only the supported version declared in the link provided by @Roman65 is acceptable. All others are not supported by GTAC and they will not help you if you have an issue. There are many dependencies and VS version is one of them. Even if you get your code to compile w/2010 then you'll likely have runtime errors that look like random events to drive you crazy. Stay sane, stay supported.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

Check my blog article on perils of mixing multiple Visual Studio versions:

 

http://siomsystems.com/mixing-visual-studio-versions/

 

---

Thanks and Regards

Yogesh Fegade

Re: Teamcenter 11, which Visual Studio Version to use (2010/2015)?.

Legend
Legend

Thank you!