02-09-2018 06:34 AM
I have Visual Studio in two different flavours, 2010 and 2015.
Which one would you use under Teamcenter 11? (ITK)
I would like to use VS2015 as its IDE colours are much more motivating, still missing the Clip, the Wizard , the Dog and Einstein that made Office so amazing in 1997. Computers and life in general are becoming increasingly boring since then.
Should I stay in VS2010 or should I go?
Solved! Go to Solution.
02-09-2018 06:39 AM
We always use certified versions,
for Teamcenter 11:
MSVisual Studio 2012 Update 1 Standard & Professional Edition with hotfix KB2781514
see there:
https://www.plm.automation.siemens.com/en_us/support/gtac/certifications.shtml#lightview-close
best regards
02-09-2018 06:45 AM
Thank you for your quick answer :)
02-09-2018 06:49 AM
But I am only allowed to choose between two flavours... 2010 or 2015, nothing in between. Some changes were made in VS2012 that affected inline functions for std and that is what scares me as I do not know if TC11 libraries were compiled in the old format or not.
02-09-2018 07:46 AM
Ok, I don't know how the TC 11 libraries are compiled (old format or not)
maybe somebody else can help here
BR
02-09-2018 09:27 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
02-09-2018 09:54 AM
Check my blog article on perils of mixing multiple Visual Studio versions:
http://siomsystems.com/mixing-visual-studio-versions/
02-12-2018 04:45 AM
Thank you!