Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter 12

Genius
Genius

When it will be realeased? Is there a list of planned new features?

5 REPLIES

Re: Teamcenter 12

Genius
Genius

Not scheduled yet?

Re: Teamcenter 12

Experimenter
Experimenter

is there any update about Teamcenter 12 release?

Re: Teamcenter 12

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Teamcenter 11.4 was released at the end of last year, Teamcenter 11.5 will be released at the end of this year, if I remember correctly, so Teamcenter 12 might be released at the end of next year.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Teamcenter 12

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The release schedule for Teamcenter follows a Spring/Fall cadence. Tc11.5/12.0 should be released soon, Spring 2018, with Tc11.6/12.1 in the Fall 2018 and Tc12.2 in Spring 2019, etc. Keeping in mind that past base releases (10.0/11.0) have been internal only with customer availability being in a later release (10.1/11.2). So depending on when the base release settles down then the customer release could be either Fall 2018 (Tc12.1) or Spring 2019 (Tc12.2).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter 12

Experimenter
Experimenter

Thank You Randy!