Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Integration Framework

Experimenter
Experimenter

What is TCIF? How is it related to T4O, T4EA and other T4X suite which Tesis developed. Are they both now combined into one single package or two different world and purpose?

6 REPLIES 6

Re: Teamcenter Integration Framework

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

It is part of the larger suite called Active Integration which includes the T4x tools (T4S, T4O and T4EA), Teamcenter Integration Framework (TcIF) and the Linked Data Framework (LDF). The T4x tools are a direct point-to-point integration (coupled) where as TcIF is an Enterprise Service Bus connection (decoupled). You use LDF to display external application data within Teamcenter. Hope that helps!


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter Integration Framework

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

T4S is meant for integrating SAP with Teamcenter and other Siemens PL products, whereas T4O is meant for Oracle EBS integration. T4EA is a generic integration tool which can be customized according to needs. These are part of Active Integration.

 

TcIF is also meant for integrating, as Randy mentioned based on a ESB and thus provides a modular approach to integration.

LDF on the other hand is different from these other frameworks, which mainly integrates using a "data exchange" philosophy, whereas LDF uses a "data linking" paradigm for integration. In many cases (specially ALM integration) the tools and underlying data model are so different that only data linking makes sense. LDF is the framework that provides the data linking capability. LDF is OSLC compliant.

 

TcIF and LDF are not part of Active Integration.

 

Best Regards

Projyal

Re: Teamcenter Integration Framework

Experimenter
Experimenter

Thanks @Projyal and @RandyEllsworth for the reply, It gave a fair idea. Im currently using T4O for integrating Oracle EBS with teamcenter. Now planning to integrate another enterprise system(quality tool) with teamcenter. In this case im stuck between choosing TCIF or T4EA. Is there are best approach or recommended way to select from these set of applications.

Re: Teamcenter Integration Framework

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

It will somewhat depend on your use-cases. But largely if there is CAD data involved use TcIF else use T4EA.

 

Best Regards

Projyal

Re: Teamcenter Integration Framework

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

@Projyal, Do you know when TcIF/LDF were removed from Active Integration? Every ECC and SPLM Conf session I've attended and all the material I've read have said that they were included.

Active.PNG


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter Integration Framework

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Randy

You are correct. But please see the following too:

AI.JPG

 

It is the future desired state. It is not a part yet. I believe there was a it of miscommunication there. I will update the collateral, thanks for bringing that to attention.

This does not affect any licensing though. Active Integration is a logical collection. The products are licensed separately.

 

Best Regards

Projyal