Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter/NX Timeline

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

We are trying to find how long does it take for the flow of the Teamcenter procedures for example when searching for an Item.

1- t=0s

User searches for an Item

2- t=0,01s

Application server sends the request to FMS

3- t=0,34s

FMS checks if the data is found the FCC

 

... and so on. Is there any method or tool to measure these timings? What would be the best way to persue the whole precedure?

 

Thx in advance!

M

1 REPLY 1

Re: Teamcenter/NX Timeline

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You could try setting these variables in tc_profilevars:

 

set TC_JOURNAL=FULL

set TC_JOURNAL_PERFORMANCE_ONLY=1

set TC_SQL_DEBUG=bJT

 

A journal file will be created for each user session (with file extension .jnl) and it will contain information about the calls made and answered, and the time it took. Better yet, you could use JournalWorkbench to view the journal files, but I think it requires a special license.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC