Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter OS migration from Solaris to RHEL

Experimenter
Experimenter

Hi Experts,

 

Can someone tell me what are all the steps to be carried out for Teamcenter 10.1.3 OS migration from Solaris to RHEL

 

* Like what are all the prerequisite required ???

* What are all the configurations to be done ??

 

 

Waiting for your valuable response.

 

Thanks !!!

5 REPLIES

Re: Teamcenter OS migration from Solaris to RHEL

Experimenter
Experimenter
Hi Experts,

Any thoughts on this ???

Re: Teamcenter OS migration from Solaris to RHEL

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
It's complicated. Are you familiar with how to clone an environment? Clone the Solaris environment on RHEL.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter OS migration from Solaris to RHEL

Legend
Legend

I do not exactly know if this will work, but you can try this option for testing:

1) Make a backup of the database, tcdata and volumes on Solaris
2) Install Teamcenter of the same version on RHEL with all the same components as on Solaris
3) Restore the backup of the database, tcdata and volumes on RHEL
4) During restore, you will also need to change some settings in tcdata and FMS, for the correct operation of Teamcenter.

Re: Teamcenter OS migration from Solaris to RHEL

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Continuing with post from Arthur3...
4a) Change the volume info in the database instance using SQL before starting.

That's a good high-level summary of the (initial) environment cloning process. Then you would need to change the rich clients to see the RHEL server.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter OS migration from Solaris to RHEL

Legend
Legend

Yes, described high-level without details.
I can also add that this way we moved the Teamcenter installation from Windows to Windows, but I think that the same thing should work for Solaris and RHEL, as well. as I understand it, both UNIX based systems
.