Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter Workflow Process

Creator
Creator

Looking for a way to remove the workflow completly using the workflow handlers. We have a workflow that progresses datasets through checks and approvals, but has a reject path, and a condition that allows the engineers to either modify the contents of the workflow or remove them. If the remove them all the status is stripped, but the workflow process is left on the items, it is this I would like to have removed to complete the loop, so it becomes self maintaining, rather than await dba to remove the workflow process which is now in fact empty

2 REPLIES

Re: Teamcenter Workflow Process

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
In your workflow rejection path you can add EPM-remove-objects handler, if status is present then you can add set-status DELETE.
Best Regards,
Jeethan Rohan

Re: Teamcenter Workflow Process

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Hi,
I believe your issue is solved, If not please feel free to contact.
Best Regards,
Jeethan Rohan