Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Teamcenter compatibility with WIN 10

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I would like to know which is the lowest version of teamcenter that is compatible with Win 10 (64 Bit) and from Siemens Supported. I couldn't find anything in the Matrix about Win 10, only Win 7 oder Win Server.

 

Thanks in Advance!

5 REPLIES 5

Re: Teamcenter compatibility with WIN 10

Siemens Phenom Siemens Phenom
Siemens Phenom
At Tc11.2.2 – All clients are supported on Windows 10 (Pro & Enterprise using CBB updates)

Prior to Tc11.2.2, Only AW 3.0 Client supports Windows 10 (Pro and Enterprise using CBB updates)

Does this help?

Re: Teamcenter compatibility with WIN 10

Legend
Legend

TC 10.1.5 not supported for Windows 10?

Re: Teamcenter compatibility with WIN 10

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Windows 10 support for Teamcenter 10 is from 10.1.6

Re: Teamcenter compatibility with WIN 10

Legend
Legend

Yes, but I noticed that 10.1.5 works fine too on Win10

Re: Teamcenter compatibility with WIN 10

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
But not the "support" part of the requirement. For Siemens support, you'll need to be compliant on the support version. It works with Tc10.1.2 also.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4