Showing results for 
Search instead for 
Did you mean: 

Teamcenter integration with NX



When I try to start NX in TeamCenter, Cattura.PNG

I think because need to install feature NX integration in Teamcenter on rich-client, but when i try to install this feature, in installation ask me the root of installation NX



This is message when i try to install the feature.


On my client and Server are installed TeamCenter

On Client is installed NX 10

On server I installed extension of integration of NX, but there is not NX installed. (I have to install NX also on Server?)

Before I thought that problem was a version of teamcenter (i had installed 10.1.0), and I proceeded to update at a version, but the problem not is solved.


How should I do for install feature of integration of NX?


Thank's for Replay.