Cancel
Showing results for 
Search instead for 
Did you mean: 

Teamcenter preferences for Multi-Cad configuration:

Pioneer
Pioneer

Hello I am trying to perform the multicad configuration for the integration of NX. Part of the configuration need to be done in the teamcenter preferences...

According to the help of NX (see next picture) I have to set those preference as they explain in the picture...

teamcenter preferences.PNG

 

My problem is with the ones that are underlined in the picture because they dont appear in my teamcenter preferences...so I do not know what to do ...

I saw that I can create a new preference definition but I need to know what category should I use for them ...

tc_pr.PNG

 

Any idea what to do here?

 

Thanks a lot 

Regards

2 REPLIES 2
Highlighted

Re: Teamcenter preferences for Multi-Cad configuration:

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
These are JT specific preferences and be created without a category. If you are using "foreign" datasets in NX (like JT) then you may need the first pref. If you are exporting/importing JT's then the position pref may be required.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Teamcenter preferences for Multi-Cad configuration:

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

i add this to category General

 

--
regards
dj