Cancel
Showing results for 
Search instead for 
Did you mean: 

TeamcenterVis 11.4 vs 11.3 VRPN Controller Problem

Experimenter
Experimenter

Hello Everybody,

I use TCVis 11.3 in an immersive environment. The WiiController is connect with vrpn and it work relative good.  Yesterday I updated to TCVis 11.4, same Hardware, same configurations but the Button events of the controller do not reach TCVis 11.4. Sometimes I have one event it is triggered.

In the menu point Concept->Sensors I see the events so my vrpn configuration is right. 

I think it is a bug in 11.4, have anybody the same problems or a solution? Thanks!