Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Templates

Genius
Genius

templates are stored in your default dba(you may know which account) home directory. you can delete and import updated one.
I did recently.

Re: Templates

Genius
Genius

Hi. 

 

The original owner is 'infodba'.  The owner to rev 'b' is me.

 

Could this be the cause?

Re: Templates

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The Checkin/Checkout privilege is grayed out. Meaning you do not have that permission.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Templates

Gears Phenom Gears Phenom
Gears Phenom

1) You can add an object ACL for CheckIn / CheckOut for full rights. Add a check mark for CheckIn / CheckOut.
Then you can also go in and delete it here. Do not forget to restart SE after changing the permissions.

large.jpg


2) You can try creating a new revision in SE by logging into Teamcenter as infodba

3) I still do not really like the idea of doing a second revision for the template, usually the existing template is updated or added new (in the new Item) - so usually I do for NX. With SE, I did not work, maybe there you can do revisions for template.

Highlighted

Re: Templates

Genius
Genius

Hi.

 

I cannot login as infodba because I do not have the password.

 

It seems I will just have to fully update our template and add as a new item.