Cancel
Showing results for 
Search instead for 
Did you mean: 

Total quantity of a single part in a multilayer assembly

Experimenter
Experimenter

I am making a different kind of bill of materials.
I want to know the total weight of a material in a multilayer assembly.

For this I need the total count of each item.

I want to use the structure manager for this.
For example the slide runner plate (selected in blue) has a quantity of 1. But it is in a sub-assembly with a quantity of 2. So the total quantity of the slide runner plate is 2.
Is there a way to add a column that would say total count? Then when I export it to MS Excel I can use this to calculate the total mass of st 12-03 with a pivot table.

I work with Teamcenter 9.

 

Capture.PNG