Cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer Mode For Exporting all Parents For a Child

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I am able to export all the parents for a child within a BOM.

How do I export all the parents for that child which belog to different BOMs

 

Thanks

Atul

15 REPLIES 15
Highlighted

Re: Transfer Mode For Exporting all Parents For a Child

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You have to perform a "Where Used" on the child to find all of its parents. You can select the parents and paste them into your Home folder (or a subfolder). Then select the objects in the folder and Export.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Transfer Mode For Exporting all Parents For a Child

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks Randy.

 

I am looking for the transfer mode so that I can create a Tc report based on it.

Looking for the right mode or a custom one.

 

Thanks

Atul

 

Re: Transfer Mode For Exporting all Parents For a Child

Valued Contributor
Valued Contributor
You mean a transfer mode to simulate a where-used on selected object till the last level without context of a particular BOM ?


________________________________

Re: Transfer Mode For Exporting all Parents For a Child

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Yes

Re: Transfer Mode For Exporting all Parents For a Child

Creator
Creator

Hello,

 

 

CLASS:ItemRevision:CLASS:Item:PROPERTY:items_tag:TRAVERSE
CLASS:Item:CLASS:PSOccurrence:REFBY:*:TRAVERSE
CLASS:ItemRevision:CLASS:PSOccurrence:REFBY:*:TRAVERSE
CLASS:PSOccurrence:CLASS:PSBOMViewRevision:PROPERTY:parent_bvr:TRAVERSE
CLASS:PSBOMViewRevision:CLASS:ItemRevision:REFBY:structure_revisions:PROCESS+TRAVERSE

 

Re: Transfer Mode For Exporting all Parents For a Child

Creator
Creator

I tried with above closure rule and it works very fine. 

Next challenge is using the appropriate property set to filter out the required aggregates to be reported.

 

Thank you.

Re: Transfer Mode For Exporting all Parents For a Child

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks!

 

It works!

Re: Transfer Mode For Exporting all Parents For a Child

Creator
Creator

Hi,

 

Are you able to export/process the relation between the child and the parent? With the above transfer mode, we are able to find all the parents. However, we are not able to connect the parents with child.

I'm expecting some GeneralRelation node in the xml output.

Re: Transfer Mode For Exporting all Parents For a Child

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

You can try combining CRF PS BOM Structure closure rue with this one to achieve the relationship