Cancel
Showing results for 
Search instead for 
Did you mean: 

Transient Volume location for 2 tier TC connection

Experimenter
Experimenter

Hi Experts , 

         I have a problem in uploading a file on Transient volume.

Problem Description :

    2 Tier Connection: 

My client application is using two tier (IIOP) connection to upload file into transient volume.But its using current node (where server is running) temp location is used. But i want to make  use  of actual transient volume location on registered node using FMS master file and  Transient  volume preference. Because  i am going to access this file using another place using   ticket. 

     4 tier Connection :

In this case i have no problem. Because pool server is consuming actual registered transient  volume. So i can access the uploaded file from any where using ticket.   

                                                       

   I am looking for the solution in which i can use actual transient volume irrespective of 2 Tier /4 Tier.Kindly help me if have any ideas.

 

1 REPLY

Re: Transient Volume location for 2 tier TC connection

Experimenter
Experimenter

Used below APIs to upload and download file on Actual  Transient Volume. 

IMF_get_transient_file_write_ticket( SS_TEXT,4, path.c_str() , &writeTicket)

IMF_get_transient_file_read_ticket(SS_TEXT,4,false,ticket_file_path,&readicket)