Cancel
Showing results for 
Search instead for 
Did you mean: 

UPDATE SWIM11.2 INTEGRATION

Pioneer
Pioneer

Dear All

I have an update Teamcenter Integration for Solidworks2016 (SWIM11.2) my TC spec:

1. Teamcenter 10 (10.1.2.1)

2. Teamcenter Integration for Solidworks 2016 (SWIM11.2)

 

after update i have some problem :

1. Local working status is Read Only  (C:\\apps\swim_data)

2. Save file solidworks with checklist JT file, but JT file can't save in to Teamcenter.

 

Please Help this case.

 

Thank You

Sudikin

Administrator Teamcenter

SW Integration 2016

3 REPLIES 3

Re: UPDATE SWIM11.2 INTEGRATION

Pioneer
Pioneer

Quest : 1. Solving, case OK

            2. Waiting any suggest...

Thanks

Re: UPDATE SWIM11.2 INTEGRATION

Legend
Legend

Answe to 2)

I hade the same issue as you with JT.

Reported it to GTAC and meanwhile I found the root cause. There are some extra space in one file that can't be read by the JT translator. You will see it in if you try to run the jt translation manually in command prompt that it report filepath is wrong. The files the conversion is creating for it are generated under your tempfolder (%temp%) .

 

... to solve the issue change the file swtojt.txt located under [SWIM DIR]\swjt so the extra space after each row is removed.

You can also read it on GTAC https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=swtojt.txt+&file_type...

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018

Re: UPDATE SWIM11.2 INTEGRATION

Pioneer
Pioneer
Hey Jormah I created in file swtojt.txt like this : {eai_config_file} {cad_file} And this working. Thank You