Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Uninstalled and reinstalled Acrobat Reader: "unable to open dataset. no compatible tool" ?

Genius
Genius

Hello

I uninstalled and reinstalled Acrobat Reader: (and restarted computer)

  • Now Teamcenter (11.4(20171201.00)) gives this error when trying to open a .PDF file.

"Unable to open dataset: No compatible tool is found."

  • I have tried to fix it by installing different versions of Reader: the latest DC and also older 9.1 and 9.0 but same error comes up.

error312342.jpg

4 REPLIES 4

Re: Uninstalled and reinstalled Acrobat Reader: "unable to open dataset. no compatible tool&quo

Genius
Genius

The error is still there:

Outside TC11: Windows 10 opens the PDFs correctly and Acrobat Reader-software is set as a default .PDF opener inside Windows.

But when trying to open PDF-datasets inside TC11: (The same error is there: "No Compatible Tool is Found".)

Is there a easy check box option to choose and set a certain PDF Reader as a default selection inside TC11 ?

- How does the Teamcenter 11 choose and autofind the needed PDF reader ?

Where is "the science" of how TC11 finds the compatible PDF opener ?

 

-------------------------------------------------------------------------------------------

I found this below "guide" online ?

How to open PDF datasets with Foxit Reader in Teamcenter

User wants to open PDF dataset with Foxit Reader by double click.

User want the configuration settings required for this requirement.

  • Hardware/Software Configuration
  • Windows 7
  • Please perform the below steps to open PDF dataset with Foxit Reader,

 

1,Install Foxit Reader application on user machine.

 

2,create FOX.bat file in c:\ drive with following contents

    @echo off

    set FOXD=C:\Program Files (x86)\Foxit Software\Foxit Reader -you can enter

your install path

    call "%FOXD%/FoxitReader.exe" "%2"

 

In BMIDE

--------

3,Define a new dataset tool for Foxit Reader in BMIDE with following details

         - MIME/TYPE  : application/pdf

         - Shell/Symbol : c:\FOX.bat

         - Tool Input/Output: Binary

         - Tool Markup Info: Win Launch Command: FoxitReader.exe

 

4, Add this new tool to PDF dataset

   In Dataset Properties;

         - Add this new tool in Tools for Edit and Tools for View

         - Add this new tool in Open, OpenUsing in ToolActions tab.

 

5, Save and Deploy it

 

6, In User machine Registry Editor,

   perform following

   A, Select HKEY_CLASSES_ROOT->.pdf

       Enter Default -FoxitReader.Document

       Enter Content Type - application/pdf

 

   B, Select HKEY_CLASSES_ROOT->FoxitReader.Document

      Select sub key shell->open->command

      Enter Default value -Enter FOX.bat path created at step2(eg: c:\FOX.bat)

 

7, Restart TC services

 

8, clean the RAC cache under C:\Users\<user id>\RAC folder

 

9, Launch New Teamcenter session and open any PDF dataset, it will open PDF

dataset in Foxit Reader

 

 

Re: Uninstalled and reinstalled Acrobat Reader: "unable to open dataset. no compatible tool&

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The logic for what is shown in the Viewer is in defaultViewer.VIEWERCONFIG. The logic for what is launched when double-click or Open is a mixture of BMIDE (example above) or by file associations in the OS (default application).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Uninstalled and reinstalled Acrobat Reader: "unable to open dataset. no compatible tool&amp

Genius
Genius

Hello

I tried to modify regedit.exe "https://www.adobe.com/devnet-docs/acrobatetk/tools/AdminGuide/pdfviewer.html".

By adding= AcroExch.Document.2017.

 

I'll see if Windows Restore function works on this Windows 10.

  • This all happened 2 days ago when I was installing a .PDF modifier software which is now uninstalled.
  • It probably mixed up the registry "regedit.exe".

How should a working "Computer\HKEY_CLASSES_ROOT\.pdf" look like ?

 

registry.jpg

Re: Uninstalled and reinstalled Acrobat Reader: "unable to open dataset. no compatible tool&amp

Genius
Genius

Looks like installing and unistalling PDF-XChange Editor 7.0 caused this error to happen.

https://www.tracker-software.com/product/pdf-xchange-editor/download?fileid=609

 

I installed this again and now TC11 opens files in PDF-XChange Editor 7.0.

but when I uninstall it and install Acrobat Reader DC it will not open in TC11.

 

PDF-XChange Editor 7.0 messed up the Windows 10 .PDF-registry. ( and will not fix even when uninstalled. )

Computer\HKEY_CLASSES_ROOT\.pdf

reg544.jpg