Cancel
Showing results for 
Search instead for 
Did you mean: 

Update of a single JAR within JAVA

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Everybody,

 

is it possible to update a single JAR: ojdbc6.jar within JAVA?

 

Thanks in Advance!

1 REPLY 1

Re: Update of a single JAR within JAVA

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I believe that file is contained/used in the 4t rich client folder and not the java installation? See your TC_ROOT\install\install folder where all the DB connectors are stored. For example, my 4tRAC is installed at C:\Siemens\Teamcenter so the file is at C:\Siemens\Teamcenter\install\install\. Keep in mind that the jar (db connector for specific version of Oracle) and the version of Tc are tied together so be careful.

That said, I've only needed to update the web application server in the past and not the rich client nor java. And then only when configuring Global Services (BPEL). Here's the link:
https://docs.plm.automation.siemens.com/tdoc/tc/12.1/help/#uid:install_jboss

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4