Showing results for 
Search instead for 
Do you mean 
Reply

User creation in Teamcenter using SOA

[ Edited ]

Could anyone tell me how to create user in Teamcenter using SOA ?

2 REPLIES

Re: User creation in Teamcenter using SOA

Mee too

Re: User creation in Teamcenter using SOA

You can use following method:

 

UserManagementService.MakeUser()

This operation executes the make_user utility on the Teamcenter server with the specified command line arguments and optional batch input file. The make_user utility runs with the same user and group as the current session user.

Parameters

Arguments
Type: array< System..::.String >[]()[]
A list of command line arguments for the make_user utility. These arguments are specified in the same format as in the make_user utility. All make_user command line arguments are supported except "-u=", "-p=", "-g=", "-pf=" and "-file=". If unsupported arguments are specified, they are ignored.

BatchFileFmsTicket
Type: System..::.String
FMS ticket for a make_user batch input file. To run make_user with a batch input file, the client must first upload the file to Teamcenter using FMS, and pass the resulting FMS ticket as this input parameter. If the ticket is not empty, the file is passed to the make_user utility using the -file=file_path argument.

EnableStandardOutput
Type: System..::.Boolean
If true, the standard output from the make_user utility is returned as an FMS file ticket. If false, the output is discarded.

EnableStandardError
Type: System..::.Boolean
If true, the standard error output from the make_user utility is returned as an FMS file ticket. If false, the error output is discarded.