Cancel
Showing results for 
Search instead for 
Did you mean: 

Using AWC with a tablet (MS Surface)

Experimenter
Experimenter

Hi, before I go looking, does anyone know if there are specific requirments to run Active Workspace on a Tablet?

4 REPLIES 4

Re: Using AWC with a tablet (MS Surface)

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I think as long as the tablet is on your network then you should be good to go.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Using AWC with a tablet (MS Surface)

Experimenter
Experimenter

Thanks, I thought so, I just didn't want to seach for soemething that wasn't needed!!

Highlighted

Re: Using AWC with a tablet (MS Surface)

Genius
Genius

Hello @ddinner5 ,

Be cautious with the browser you're using and maybe make some tests before. When the browser is not fully compatible with HTML5 or a bit deprecated (like IE) you might have some functionnalities that are not working (Video playing for example).

If you want to use the graphical view, you might need to have some power on your tablet, even more if you'll be using "Client-side rendering".

best regards,

Frédéric.

Re: Using AWC with a tablet (MS Surface)

Experimenter
Experimenter

Thank you for that, I will absolutly do testing on different broswers, currently on Laptops, chrome is best browser so far...i don't have the tablet let but when i get i will do this first.