Cancel
Showing results for 
Search instead for 
Did you mean: 

Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Experimenter
Experimenter

Hi there,

 

did anyone do this before?

I would like to share experiences with other users, but it seems to be pioneering...

 

BR, Thomas

 

 

HC DI CV PS MD 1
10 REPLIES

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

It works in EDA 2.0.1 + Mentor Vx1.2 + Teamcenter 11.2.2 combination

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Experimenter
Experimenter

Thanks, that is nice to know.

 

Did you set up your environment yourself, according to document PLM00087 2.0.1, or with the help of PLM?

I ask because we ran from issue to issue with document PLM00087 2.0...

 

And do you have experiences with VX2 also? Because we plan to update our flow from 7.9.5EE to VX2.

HC DI CV PS MD 1

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Thomasle,

 

Sorry for late reply. It was holiday time in China. 

Yes, PLM00087 2.0 is the only document we got. 

Me too ran from issue to issue. 

We found several new issue today.   

IR 8524789, User has to manually select .edc file when saving schematic files in to TC using viewable option "From Schematic". 

IR 8523487, "decryptonly" license error pops up when creating viewable files from PCB with option "From PCB".

 

I have not tested with VX2, but from the matrix, I think it is currently not supported.

 

How is the project going in your side? you can email me at zhe.sun@siemens.com to share some experience

 

 

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Experimenter
Experimenter

Hi Sun Zhe,

 

thanks for getting back to me. I will send you my PLM00087 2.0 with comments of all the issues we ran into.

 

Unfortunally I can't access your quoted IR's, but had the same issue with the decryptonly issue.

 

Exceptionally this is a Mentor issue, as they encrypted their pcb files somewhere between EE7.9.1 and EE7.9.5 and later..

So you need to contact Mentor for providing the correct license.

 

But imho paper is patient. I ask myself if the steps in PLM00087 2.0 have ever been tested, or not, as paper is patient. So they shall have run into the same and many other issues, which cost us many efforts.

 

Btw: You are right, VX2 is not supported yet.

 

 

BR, Thomas

HC DI CV PS MD 1

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Experimenter
Experimenter

ll: just saw I could upload my commented PDF here also.

 

Maybe it helps someone..

 

Environment was EE7.9.5 + EDA2.0 + TC11.2.1

HC DI CV PS MD 1

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

 

This is mayur thange,

Currently I am working on EDA-Altium integration.

When i tryed to SaveAs Item on EDA-client, it shows me PCA & PWB type, But I required only PWB type of item.

If you have any idea regarding above please shear,please find attached image file 

 

If you have any user media or some douments please shear it, it will help me.

 

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Sorry for late reply.

I am currently working for another project. So not quite sure about the preference.

As far as I know, there is a Teamcenter preference to control this behavior. 

You can take a look into the preference "EDA_DefinedPWBWith"

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Legend
Legend

Hello Mayur,

 

No we can not stop creating any one of them, what you can do is to set custom objects by preferences for creation of this PCA and PWB.

 

On PCA, you will have you altium project dataset saved. when you save from the altium

 

and PWB component you may used for the Fabrication data, Geber files, NC drills files and data sheets.

 

So instead of avoiding PWB creation, use it..!!!

Re: Using EDA-Client (2.0) for Mentor Expedition with Teamcenter (11.2.1)

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Guys,

 

I am working with EDA Altium Integration, maybe is a bit late but I found that by modifying the TC_EDA preference EDA_DefinePWBWith as "none" it prevents the creation of the PWB item, you can refer to the attached image.This will create the BOM on your futurevariant item.

 

I am agree with Ganesh instead of avoiding PWB creation is better to use it, which brings me to this discussion Smiley Happy. Do you know how to create Schematics, PCB and fabrication datasets separately? is there any preference or config file to setup?

 

When I create a project in altium which includes Schematics, pcb, gerber and NC drill files and I execute the Save-as Command all these files are being saved in a single dataset called "EDADesAltiumBrd", and I was wondering if I can put these files in separate datasets?

 

Thanks,