Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Virtual server versus Physical server -- which works best?

Experimenter
Experimenter

@Stefan_Pendl,

 

Can we virtualize TC11.2 with microsoft hyper-v?

Re: Virtual server versus Physical server -- which works best?

Builder
Builder

@Stefan_Pendl,

 

Can we virtualize Teamcenter 11.2 with microsoft hyper-v?

Re: Virtual server versus Physical server -- which works best?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Yes you can. I run Tc11.2.2 in Hyper-V. However, some things are more difficult than you would imagine. With VMware, creating an "generic" installation and then copying it to a "specific" installation (cloning) is straight forward. For instance, creating a server that has Windows and MS SQL server (ootb) installed (the golden copy) then copying it to a new server and installing Teamcenter. This is very difficult in Hyper-V for some reason. However Hyper-V is free on all the new versions of Windows.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4