Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Visualization - How to "reset to default" after sorting my project workspace?

Experimenter
Experimenter

Hello,

 

If I'm viewing a JT assembly in Vis, and I click on one of the headers in the "project workspace" window, it sorts on that column. However, it'd be nice to be able to quickly reset it "un-sort" so that it goes back to the default ordering. Is there any way to do this without closing the vis session and re-opening it?

 

Thanks,

Will 

1 REPLY 1

Re: Visualization - How to "reset to default" after sorting my project workspace?

Siemens Genius Siemens Genius
Siemens Genius

Is the JT data managed in Teamcenter? If so, you could use the menu: File --> Preferences --> Teamcenter Integration --> Attributes to map in the Find #, add it as a column, then sort on that.

 

Keep in mind that you need to restart TC Vis for any changes to the attribute mapping to take effect.