Cancel
Showing results for 
Search instead for 
Did you mean: 

While updating the patch 10.1.6 from 10.1, do we need to replace the files from Install folder?

Hello Team,

 

Currently I am having 10.1 Teamcenter server installed on my machine, now i want to update the patch  to 10.1.6, so downloaded the Patch dumps from GTAC. My query is do we need to replace the %TC_ROOT%\install\(files/folder) , by the files which given in the dumps like shown below for 10.1.4

 

installfolder.PNG

 

when you replace these files/folder update window will be like this,

 

patch.png

 

But when i downloaded for 10.1.6 i got only one folder as below,

 

10.1.6.PNG

 

so should i go without repacing files, will it be OK?

1 REPLY

Re: While updating the patch 10.1.6 from 10.1, do we need to replace the files from Install folder?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

You always need the install files. If I log into download server I can see it.

 

2016-12-16 17_52_53-Clipboard.png

xtof