Cancel
Showing results for 
Search instead for 
Did you mean: 

Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment

Pioneer
Pioneer

Hello Team,

 

When I login into particular client, I am getting this error...

 

WARN 2016-04-05 16:07:36,114 - Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment (1.7.0-b147) - 3.8.0.v20120529-1548
ERROR 2016-04-05 16:07:36,316 - invalid code lengths set
java.util.zip.ZipException: invalid code lengths set
at java.util.zip.InflaterInputStream.read(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.XMLEntityManager$RewindableInputStream.read(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.io.UTF8Reader.read(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.XMLEntityScanner.load(Unknown Source)
at com.sun.org.apache.xerces.internal.impl.XMLEntityScanner.skipChar(Unknown Source)

 

I tried reinstalling Java, but still it gives teh same error in RAC. In Syslog there are no errors listed.

 

What could be the resons.....?

 

S A Saravanakumar
CBE, INDIA
4 REPLIES

Re: Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment

The source for that error could be a zip file containing paths that are too long for Windows (max 260 chars length). Try locating the zip file and remove, if at all possible, the offending files from it. Some zip files are generated in OS' that do not have that limit set and are the source of problems when trying to inflate them under 'JAVA'.

Re: Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment

Esteemed Contributor
Esteemed Contributor

The limit of 260 characters only applies to the ANSI API functions of Windows, the Unicode functions for paths support 32768 characters.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Try to clear .gz registry files (\TCROOT\portal\registry) and regenerate the registry again.

Re: Windows 7 (Service Pack 1) - win32.win32.x86_64 - null - Java(TM) SE Runtime Environment

Pioneer
Pioneer
Thnx!!!
S A Saravanakumar
CBE, INDIA