Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Workflow cannot be deleted or set in Edit Mode

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I just cannot try to edit a certain WF. I tried to export it from the customer's Rich Client and import it on my PC, the Edit-Mode and Delete works just fine.

 

Do you have any ideas what can I try to solve this issue?

 

How can I check where is this WF referenced?

 

2018-10-30 12_49_37-Window.jpg

36 REPLIES 36

Re: Workflow cannot be deleted or set in Edit Mode

Phenom
Phenom

If you can export and edit on your pc, then i would try just re-importing it to customers rich client.  Then try to edit it.

Richard Bennett
Prospect PLM

Re: Workflow cannot be deleted or set in Edit Mode

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@ProspectPLM wrote:

If you can export and edit on your pc, then i would try just re-importing it to customers rich client.  Then try to edit it.



Thank you for your reply,

 

I already tried to reimport it and it didn't help. The customer would like to set it offline (deactivate it) or even deleting it.

Re: Workflow cannot be deleted or set in Edit Mode

Phenom
Phenom

Have you tried where referenced POM in impact analysis?  Im clutching at straws now...

Richard Bennett
Prospect PLM

Re: Workflow cannot be deleted or set in Edit Mode

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

@ProspectPLM wrote:

Have you tried where referenced POM in impact analysis?  Im clutching at straws now...



It only Shows the Tasks inside the Workflow. Without being referenced to an Item or anything else.

Re: Workflow cannot be deleted or set in Edit Mode

Gears Phenom Gears Phenom
Gears Phenom

You selected the root template, sent to My Teamcenter, then did Impact Analysis, Where Referenced (POM)? Please show screenshot of that. 

 

Jamie Griffis, Teamcenter Architect, Applied CAx, LLC

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: Workflow cannot be deleted or set in Edit Mode

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

2018-10-30 14_40_45-Window.jpg

Re: Workflow cannot be deleted or set in Edit Mode

Gears Phenom Gears Phenom
Gears Phenom

There isn't a little binder clip in that list, which could cause problems deleting. But I don't see the "Add Checked status" as shown in your error screenshot. Is this the same root workflow?  edit: I see it now. Can you expand that task to see if there is a binder clip icon attached to it?

Jamie Griffis | PLM Solution Architect | Engineering USA

Re: Workflow cannot be deleted or set in Edit Mode

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

No difference in the Impact Analysis between my PC and that of the Customer.2018-10-30 15_07_07-Window.jpg

Re: Workflow cannot be deleted or set in Edit Mode

Gears Phenom Gears Phenom
Gears Phenom

Have you tried running verify_tasks yet? This will find all the corrupted workflow tasks and jobs. Maybe it is linked to something corrupted and this will help clear it up. 

Jamie Griffis | PLM Solution Architect | Engineering USA