Cancel
Showing results for 
Search instead for 
Did you mean: 

question about Variation simulation analysis

Creator
Creator

Hi, I am studying VSA in teamcenter.

 

I did a simple assembly, with 2 blocks assembled perpendicular to each other

 

then I bring them into TeamCenter process document

 

I add 3 VA elements  1) one contact plane between 2 blocks, 2) one VA plane on the vertical block  3) one VA plane on the horizontal block

 

 

i want to measure the angle between these two blocks based on the input tolerance,

 

But I got error mesage

 

Honestly, I just went through the only one tutorial in TeamCenter help, so I am a green man...

 

 

Can anyone help me achieve this goal, I attach file

I am running TC 9.1

 

thank you

 

 

Capture1.JPG

2 REPLIES

Re: question about Variation simulation analysis

Experimenter
Experimenter

Hi,

 

Just switch on abosulute icon in the measument window under direction vector.

 

 

Re: question about Variation simulation analysis

Experimenter
Experimenter

Hi

 

I am using 10.1 & I am able to create measurement too

 

Pls check and let me know, your findings

 

Thanks,

Yuvraj