Cancel
Showing results for 
Search instead for 
Did you mean: 

set field width in the rendering stylesheet

Experimenter
Experimenter

Hello,
I would like to make the field width smaller in the rendering stylesheet, because only one number is entered here. As soon as I check out the revision, a fixed field width is always displayed.
Attribut.png

<section titleKey="tc_xrt " >
<column>
<property name="la4_fertigung"/>
<property name="la4_einkauf"/>
</column>
</section>

 

How can I configure this?

2 REPLIES 2

Re: set field width in the rendering stylesheet

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
How about adding "width=20" to the property arguments and adjust from there?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: set field width in the rendering stylesheet

Legend
Legend

You can also try if the property is just a text field but it is going create a box (adjust column size accordingly)

 

Capture.PNG

 

<property name="la4_fertigung" renderingHint="textfield" column="10" />

Regards
Rafa