Cancel
Showing results for 
Search instead for 
Did you mean: 

tcexcel_import utility

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi

 

Wondering if somebody has an experience on this. I started to use tcexcel_import utility to create some structures I need. I have three specific problem:

1. It is not possible to create nedted activities within operations. as soon as I put two MEActivtiy Item in the excel it will generate error. look at this:

 

Header1 Item Item Item Item Item Description
Header2 Mfg0MEPlantBOP Mfg0MEProcArea MEOP MEActivity MEActivity  
Header3 Mfg0MEPlantBOP Mfg0MEProcStatn MEOP MEActivity MEActivity  
Title Root Station Level Operation level Activity level 1 Activity level 2

Description

 

2. I can update time attribute of an activity but this will end up in "duration" attribute and not the "unit time". Also couldn't find a way to update the frequency of an activity.

 

3. How can I add attributes such as estimated, allocated time for a Process Station item?

 

Header1 Item Item Item Item Attribute Attribute
Header2 Mfg0MEPlantBOP Mfg0MEProcArea MEOP MEActivity ItemRevision Master ItemRevision Master
Header3 Mfg0MEPlantBOP Mfg0MEProcStatn MEOP MEActivity Estimated Time Allocated Time
Title Root Station Level Operation level Activity level 1