Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM Reuse Library Samples: download setup hardware and work-holding devices

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Works with NX Version: NX 8
CAM Reuse Library Samples Version: Workholding_8.a.1

 

(view in My Videos)
 

Tech Tip by Michael Mannino, Siemens PLM Software

Description
The zip file, CAM_Reuse_Library_Samples.zip, contains the files (prt, xls, krx, bmp) needed to install a sample set of reusable setup hardware and work-holding devices useful to NC programmers using NX CAM. Follow these instructions below to add this sample library to your NX Reuse Library.

Sample Library Contents

  • Setup hardware (angle plates, bushings, cap screws, C-clamps, clamp strap blocks, clamp straps, I-parallels, modular-plates, parallels, pull studs, rectangular blocks, round standoffs, T-bolts and nuts, threaded studs, V-blocks)
  • Work-holding (3 jaw chucks, air chuck, collet adapters, milling vise, tombstones)
  • All parts in the sample library are English units (inch) parts


Download

  • Download the zip file attached to this Tech Tip, CAM_Reuse_Library_Samples.zip .


Installation Instructions

  • Extract the contents of CAM_Reuse_Library_Samples.zipinto an accessible folder on your computer (example: D:/CAM Reuse Library). Note that if you want to share this library with your group, you can extract the contents to a shared folder on your network.
  • Start the NX 8application.
  • Click File --> Utilities --> Customer Defaults.

1a-Customer Defaults-small.png

 

  • In the Customer Defaults dialog under the Gateway section, click Reuse Library.
  • In the General tab, under Native NX in the Libraries Organized by Native Folder section, enter the path to the top folder of the extracted files (example: CAM Reuse Library Samples | D:/CAM Reuse Library). The string before the "|" is the library name, the string after is the path. Note that the path in NX uses a forward-slash "/" to separate the folders in the file structure. Click OK.

2a-Reuse Library-small.png

 

  • Exit NX.
  • The next time you start NX, CAM Reuse Library Samples will be loaded in your Resource Bar under the Reuse Library.


Instructions for Using the Components in the Reuse Library

  • Start the NX 8application.
  • Open an existing CAM setup.
  • Start the Modeling application and turn on Assemblies.
  • Access the Reuse Library from the Resource Bar.

2.5a-Reuse Library.png

 

  • Expand CAM Reuse Library Samples then expand Hardware. Click the For Setups folder. Expand the Member Select pane.

3a-Installed Samples-small.png

 

  • Drag and drop the C-Clamp into the graphics window.
  • In the Add Reusable Component dialog, specify the Primary Parameters. (You can also change the Values in the Details area by double-clicking the value and entering a new value.) Assemble the component into your CAM setup as necessary. Click OK.

 

Do you have a question?

Click 'Add a Comment' below to ask it. (You must be signed in to use this feature.)

 


You can find more information about the Reuse Library in NX Help under Data Reuse --> Reuse Library.

Make Better Parts Faster!
Aaron Frankel (Community Manager)
Comments
Theorist
Theorist

Hello sir ,

Its really help me .

Thank you very much.

Imran.

 

Experimenter
Experimenter

Shall I use this folder in NX8.5. If not could you please provide the file for Nx8.5

Pioneer
Pioneer

Hello,

i also try this tip with 8.5.3.3MP04 but it doesn work. Need i do something more with 8.5 ??

thx

Siemens Genius Siemens Genius
Siemens Genius

ScreenHunter_03 May. 04 16.45.gif

Should work in all of NX8, NX8.5, NX9, and NX10, are there any errors or warnings produced?

 

Pioneer
Pioneer

Hello Michael,

 

thanks for the quick answer.Today i try it again at work.I forgot that we use a PLM Software. I saw that the example is for "Native NX".Is there a solution to use the example in combination with a PLM ??

 

I am not shure that the warning i am get.

"The family member saving directory does not exist"

 

thx

Siemens Genius Siemens Genius
Siemens Genius

I am not a TC solution consultant, so I am not sure on an answer. I did ask one of my colleagues, he said it may be that some of the files required for reuse are not registered in TC.

Siemens Dreamer Siemens Dreamer
Siemens Dreamer

Nice, this still works in NX11.

Are there also mm-examples available?

Contributors
LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.