Cancel
Showing results for 
Search instead for 
Did you mean: 

Easily output the name of the postprocessor file into shop documentation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Overview

Editing the postprocessor using the new command MOM_set_attribute allows the program or operation attributes to be automatically added when the operation is postprocessed. Shop Docs can then output the name of the postprocessor output file (PROGRAM.ptp file) by customizing the shop doc template.

 

Adding CAM attributes for shop documentation in the post.gif

 

Created with NX CAM 9

 

Details

The new functionality in this project is the ability to edit the postprocessor using MOM_set_attribute so that the object attributes are automatically created in the part file when the operation or program is postprocessed.

 

To use this self-demo, save the attached files locally and follow the instructions in the pdf document.

 

Do you have a question?

Post your questions or comments at the bottom of this Tech Tip. (You must be signed in to access this feature.)

 

About the Author

Holder.jpg Bill Storrs is in the CAM Product Management Group at Siemens PLM software, Cypress California. His main focus is on CAM usability and learning support. He currently leads the CAM Learning Initiative Team whose mission is to provide users with a comprehensive collection of reference and training materials. He has an M.A. in Corporate Training and Development and has been in the industry for over 20 years.

 

Comments
Solution Partner Enthusiast Solution Partner Enthusiast
Solution Partner Enthusiast

Nice!

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

If possible Could you please share more infomation for customise shop doc for excel format.

Mostly customer would like to custom report each company.

If you can share how to link $mom.... in excel to NX CAM infomation .

That is will much more better .

Or If you have VDO how to custom shopdoc as easy please let us know.

Thank you a lot.

Creator
Creator

 how to define maximum range depth in shop doc.

Creator
Creator

Can you only use this command to write attributes to the operation object?  I tried writing an attribute to the Tool object but got an error.

 

-David

VIP
VIP

Just following up here - This command is for operations and program groups only.

This was answered in the discussion forum when it was asked there: http://community.plm.automation.siemens.com/t5/Discussion-Forum-NX/mom-attr-TOOL-lt-name-gt-or-ug-se...

 

Creator
Creator

When using the MOM_set_attribute command can you specify the attribute Category?

 

Thanks,

David

Experimenter
Experimenter

Sir I want that my file name after postprocess should be default as program name , how can I do it