Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create inspection-ready programs in NX

Siemens Genius Siemens Genius
Siemens Genius

Overview

Learn the basics about NX CMM Inspection Programming and how to use it to automate programming, capture best practices, and minimize on-machine prove-outs.

 

(view in My Videos)

 

Details

  • Create an inspection template to capture best practices and the machine setup
  • Use automation tools such as Product Manufacturing Information (PMI) and CMM add-ons to reduce programming time
  • Use simulation and collision avoidance to minimize on-machine prove-out

 

Do you have a question?

Click 'Comments' below to ask it. (You must be signed in to use this feature.)

 

Make Better Parts Faster!
Aaron Frankel (Community Manager)
Comments
Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: What kind of report generators do you have for the post-processed info?

A: Measurements can be reported in three different formats:

  1. text reports
  2. csv files (Excel sheets)
  3. dml files which can then also be used to create additional reports.

The CMM Analysis Tech Tip includes more information on measurement results:

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: Are the post processors developed and editable using the Post Builder?

A: The posts are not developed in Post Builder, but are made with the standard .tcl files that are familiar to NX CAM post writers.

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: Which version of NX are we seeing here? What version will have the analysis capability?

A: This Tech Tip was demonstrated in NX 8.5, which was just released. The Analysis capabilitiy is first available in NX 8.5.0.1

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: What additional licenses would be needed for this ability?

A: The CMM Inspection Programming package in NX includes CAD capabilities, PMI tools, and the CMM programming and simulation tools. The new Analysis capabilities are included in the same CMM Inspection Programming package, and does not require any additional license.

Community Manager Community Manager
Community Manager

This question was asked during the live event:
Q: What type of fixturing is supported? Rayco, R&R, etc.

A: Any NX Assembly items can be included as fixturing. The NX re-use library can be used to provide standard fixturing components.

More info is available on the Re-use Library in the Tech Tips on this topic:

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: Do you recommend a preferred Teamcenter application for storing CMM inspection data?

A: The DMIS (or other format) CMM programs can be vaulted, or stored in Teamcenter, if that is in use. Dimensional Planning and Validation (DPV) will store measurement data in Teamcenter, then provide the opportunity to create lots of reports.

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: Is the NX CMM inspection programming module associative to NX CAD?

A: Yes. The NX CMM programs are built on the NX CAD models and completely associative.

Pioneer
Pioneer

is there an instructional video that details how to create a standardized template we can use every time we start a new job?

 

 

LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.