Cancel
Showing results for 
Search instead for 
Did you mean: 

How to make the best use of CAD for NC Programming

Siemens Genius Siemens Genius
Siemens Genius

Overview

Learn how to use the NX CAD tools to support your NC programming processes, making it easy to.

 

(view in My Videos)

 

Details

  • Import data
  • Clean up and simplify imported data
  • Create NC setup and fixture assemblies
  • Manage derivative models such as castings and work-in-progress models
  • Keep it all associative with the master model concept

 

Do you have a question?

Click 'Comments' below to ask it. (You must be signed in to use this feature.)

 

Make Better Parts Faster!
Aaron Frankel (Community Manager)
Comments
Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q: Is the model used in this demo an original model, or an imported STEP model?

A) This model was imported from Catia v5. In the aerospace industry, we see quite a bit of Catia imports, and they have certain idiosyncrasies, such as all the holes come through as split holes. So the techniques we used can be very helpful in straightening out geometry like that. By “optimizing” the model, we get single cylinder faces, as an example. Blends are sometimes represented with additional faces as well, and re-blending to the same size will reset them to single surfaces.
Of course we can import IGES, STEP, DWG, and other file types as well. The slide we showed at the beginning listed all of the file types that can be imported:

 

ImportFileTypes.png

Community Manager Community Manager
Community Manager

This question was asked during the live webcast:
Q) If I import a STEP model, will I have the same control over the model?

A) We showed several types of simple “Synchronous Modeling” optimization changes, but there are pretty significant capabilities even beyond these, that you can use on any type of model, including imported models.
Not only can we do simple things like delete or extend faces, and re-size blends, we can also re-order features in where they occur so that we can make other changes to geometry. This lets us get beyond just the topology of faces, but really lets us establish “parametric” relationships even at the topological level with synchronous technology. So there are pretty deep model preparation capabilities with these synchronous tools.

LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.