Cancel
Showing results for 
Search instead for 
Did you mean: 

Learn about the new capabilities in NX CAM 9 Holemaking

Community Manager Community Manager
Community Manager

Overview

NX CAM 9 includes new process capabilities in the Holemaking application, integrating the feature table as a selection mechanism for producing drilling, reaming, tapping, etc. operations even in the absence of full feature-based automation. Further, the new in-process volume preview has been integrated into the Holemaking operations so that it is always clear that sequences are working properly and efficiently.

 

(view in My Videos)

 

Created with NX 9.0

 

Details

Tom Van't Erve presents the new NX CAM 9 updates for Holemaking:

  • Selection based on features
  • Process vizualization

Note that this webinar recording is a partial capture of Tom live Tech Tip session, which covered both Turning and Holemaking.  The Turning portion of the session is provided in a separate recording:

http://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX/Learn-about-the-new-capab...

 

Do you have a question?

Click 'Add a Comment' below to ask it. (You must be signed in to access this feature.)

 

About the Presenter

 

Tom van 't Erve 83x110.jpg

Tom van 't Erve is the Director of Development for NX CAM Prismatic Parts Machining within Siemens PLM Software. In his role, Tom is responsible for NX CAM 2.5D Milling, Turning, Drilling, Wire EDM and Feature-Based Machining as well as the Tecnomatix Machining Line Planner. In 2005, Tom joined UGS through the acquisition of Tecnomatix, where he was responsible for the development and support of the Automotive Powertrain solution. Tom holds a MSc and a PhD degree in mechanical engineering from the University of Twente in the Netherlands.

 

Derek Hart
... if we're not having fun, we're not doing it right!
Comments
Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Do you have any examples of deep hole drilling or gun-drilling automation?

Contributors
LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.