Cancel
Showing results for 
Search instead for 
Did you mean: 

MRL - Using Boring & other adjustable tools in the Manufacturing Resource Library

Siemens Theorist Siemens Theorist
Siemens Theorist

Overview

This guideline demonstrates possible procedures for the data management system Teamcenter (TC) and the NX CAD/CAM system to better support adjustable boring tools. These modular tools offer the ability to change their cutting diameter after being assembled. This functionality should be supported by the 3D models of these tools in NX and should be controllable by changing relevant attribute values of the TC Manufacturing Resource Library (MRL).

 

P1.png

 

For each classified tool from the MRL there are two 3D models in NX:

  • The detailed 3D model (mostly provided by the tool manufacturer), which consists of the 3D data of the assembled components and is used for the simulation of material removal and collision control.
  • The parametric model, which NX CAM software generates from MRL attribute values and is used to calculate the tool path.

After changing the tool diameter value in TC Resource Manager (RM), the two 3D models in NX should automatically adjust to the new value. The individual steps to enable such functionality are explained in this guideline.

 

By default, only the diameter of the parametric model will be transferred to NX. The diameter of the detailed model will not change with it. The two models, when loaded from TC RM into the NX CAM session, would appear as shown below:

 

p2.png

 

After implementing the changes according to the guideline, the Cutting Diameter of the Detailed and Parametric Model will be synchronized automatically:

 

p3.png

 

Hands-on Demo

Save the attached part file to your local driver and follow the instructions in the PDF document.

 

Do you have a question about this topic?

Post your questions or comments at the bottom of this Tech Tip. (You must be signed in to access this feature.)

Contributors
LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.