Cancel
Showing results for 
Search instead for 
Did you mean: 

Merge Tool Paths

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 

 

Merge Tool Paths

NX CAM

 

Multiple operations can now be combined into a single operation containing a single merged tool path.

 

(view in My Videos)

 

(If you have problems with the embedded player, you can download the attached .mp4 file.)

 

Do you have a question about this topic?

Post your questions or comments at the bottom of this Tech Tip. (You must be signed in to access this feature.)

 

About the Author

BillStorrs.png Bill Storrs is in the CAM Product Management Group at Siemens PLM software, Cypress California. His main focus is on CAM usability and learning support. He currently leads the CAM Learning Initiative Team whose mission is to provide users with a comprehensive collection of reference and training materials. He has an M.A. in Corporate Training and Development and has been in the industry for over 20 years.

 

 

Comments
Creator
Creator

Hello, this is what version of Nx, where I find this is in the creation of operation?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In Siemens NX (1847) released January 2019, it is a new program order group type.

Creator
Creator

Nice to see this in NX.

 

Exactly 3 years ago, I wrote an App for Narrow channels which is still in use, to program 3-5 axis contour toolpaths in a desired step milling pattern to support variable level, variable step, variable depths. This also aids lights-out machining. Serves as an alternative for Sequential mill Looping option. Could introduce spring passes at needed areas . All of this in a simple interface with editing capabilities..

 

- Vasanth Sivanatarajan

Creator
Creator

@billstorrs Is it possible to share your sample part file which was showed in the video?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

I tried to use this nice feature but I don't get the expected result. The trajectory obtained is not different from the sequence of my 2 initial operations

 

I am using NX1851 release

 

In which release does it work?

 

Regards,

Franck

Enthusiast
Enthusiast

Hello,

 

I tried to use this feature "MERGE_PATH" in NX1872.

I tried to combine 2 operation, one with 10 steps in depth and one with 40 steps in depth.

The operations are made as 5-axis variable contour and both are correct.

I choose "Contour Count" and filled in a lot of different combinations in the table but none of them worked out.

Each combination gives me only a "Concatenation" of these files.

Do I have to put a special variable in NX or what do I do wrong?

I started with a 5-axis Multi Blade operation to rough and finish but the same result as the other operations.

 

Regards,

 

Wim Poirters sr.

 

 

Enthusiast
Enthusiast

Problem solved with "Merge_Path".

 

Date : 12-aug-2019
We solved the issue with "Merge_Path".


There is a preference setting that's causing the problem that it's not working!
In "Manufacturing Preferences" there is a setting called "Do Smart Regeneration when Possible" and this should be "ON"!


Now the "Merge_Path" is working as designed.

Regards,

Wim Poirters