Cancel
Showing results for 
Search instead for 
Did you mean: 

Python Parser Customization in NX CAM Simulation - Video training series

Community Manager Community Manager
Community Manager

Overview 

The following video training series explores the details of Python parser customization in NX CAM Simulation.

 

Basic knowledge and understanding of NX CAM software, NC Code, Python, Regular Expressions and the CSE is required.

 

If you are a beginner with the Common Simulation Engine, it is recommended to start with the introductory training videos found here:

 

Understanding Machine Tool Simulation Concepts

  

NOTE: It will take almost a minute before all of the content on this page is displayed and you can scroll down. Please be patient while the previews for all videos are loaded.

 

Created with NX 11.0.2

Details

Contents: This video series is broken down into 3 sections, as described below.  It is helpful to go through them in order at first, but having several chapters makes it easier to return to the material for reinforcement.

Learning Objectives:

  1. Gain an understanding of Python parser customization in NX CAM Simulation
  2. Become familiar with PLY module in CSE
  3. Learn on a generic sample the basics to add and customize Lex and Yacc functions 

Demo File Preparation: Save the attached sim08_mill_5ax_handson.7z file (found at the bottom of the article) locally and follow the instructions in the Session 2: Hands on sessions - 00:00:10 - First Steps: Preparing Hands On Environment

The used CAM setup and sample NC Code file is located in sim08_mill_5ax\cam_setup\

The provided sim08 sample machine found in the zip file is modified and should be used for this video series.

If you want to concentrate on the videos without coding, there is an MCF file (MyController_MCF_ToBe.7z) and the python scripts (MyController_PythonScript _ToBe_Basics.7z) with all shown modifications inside. This file is located in the sim08_mill_5ax\cse_driver\MyController\ folder.

 

Session/Chapter Overview

 

Session 1: Introduction, Overview and Theory

00:00:00 - Introduction/Overview

00:01:08 - Theory: About Parsing

00:04:57 - Theory: Configurable Parser Architecture in CSE

00:10:48 - Theory: The Lex script

00:13:07 - Theory: The YACC script

00:19:41 - Theory: CSE Python Interface

You can also find this video on YouTube, Python Parser Customization: Introduction

 

(view in My Videos)

 

Session 2: Hands on sessions

00:00:00 - Introduction

00:00:10 - First Steps: Preparing Hands On Environment

00:02:12 - First Steps: Checking Syntax

00:04:14 - First Steps: G0 X100

00:15:37 - First Steps: G0 X=100

00:21:55 - First Steps: Adding new axis address

00:23:59 - First Steps: Token Sequence

00:29:43 - First Steps: Adding 'AnyCommand'

00:33:39 - First Steps: Adding parameter to 'AnyCommand'

00:37:53 - First Steps: Adding optional MCParameter to 'AnyCommand'

00:52:18 - First Steps: NC Variables

You can also find this video on YouTube, Python Parser Customization: Hands on Sessions

 

(view in My Videos)

 

Section 3: Debugging

00:00:00 - Introduction and Overview

00:00:33 - Debugging - NX Log file

00:01:28 - Debugging - Lex sequence checker

00:07:31 - Debugging - PLY Logger

00:08:44 - Debugging - Runtime Debugging (will be submitted later)

You can also find this video on YouTube: Python Parser Customization: Debugging

 

(view in My Videos)