Cancel
Showing results for 
Search instead for 
Did you mean: 

Reduce clicks during Cut Area selection

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Overview

This Tech Tip shows some helpful shortcuts for selecting lots of geometry.

 

Selecting cut areas manually, either in operations directly or in Mill_Areas etc, is pretty easy when there aren't many surfaces.

But when you need to select several 100 surfaces or have features which you see again and again, the following will show you a few tricks on how to limit your clicks and make the cut area selection easier.

 

38.jpg

 

This Tech Tip was prepared with NX version 8.5

 

Details: Selection by color
 

Using color selection of course requires that you have different colors on your part, reflecting either features or certain part areas.

The colors can come directly from the CAD team, or you can add them in the CAM process.

 

Steps:

 

In the Specify Cut Area dialog, open the Filter Methods drop down list and choose More...

36.jpg  

Click Type button and select Face, then click OK
Click Color
If you know the Color ID number, input it in the ID field and press Enter on your keyboard.
If you do not know the Color ID number, you can click Inherit From Object and select one of the part surfaces with the color you want to have selected.

37.jpg

  
Click OK until you are back at the Cut Area dialog
Click Select All

38.jpg

 

Now your surfaces have all been selected! 

 

Details: Selection by face NAME

 

Using face NAME selection requires that you have face names on your part, reflecting either features or certain part areas. The names can come directly from the CAD team, or you can add them in the CAM process.

39.jpg

Steps:

 

In the Specify Cut Area dialog, input the name in the Name field

40.jpg

 
Press Enter on your keyboard

41.jpg

 

Now your surfaces have all been selected.

 

Additional information

 

You can reduce the user clicks even further by creating macros that assist you during the cut area selection process. To have a fully automatic macro without user interaction, it requires that either your colors or names are identical every time. Meaning you need to decide on a standard for your parts/features. If you are not able to decide on a standard, you can create macros with user-interaction.

 

The user action could in that case either be:

  • Adding the color ID number
  • Choosing the color by inheriting from object
  • Inputting the name in the name field.
  • Or similar…

 

Do you have a question?

Click 'Add a Comment' below to ask it. (You must be signed in to access this feature.)

 

About the Author

 

Lars Lars Okkels is in the Manufacturing Business Group at Siemens PLM Software and focuses on part manufacturing solutions especially for Mold & Die. He has been in the industry for over 15 years and enjoys supporting NX users applying innovative manufacturing technology solutions. Lars is originally from Denmark and now resides in Shanghai, China, with his family.

 

Lars Okkels
MBG
LIVE Tech Tip Webinars
Watch NX experts demonstrate manufacturing best practices. Stay online for Q&A.