Cancel
Showing results for 
Search instead for 
Did you mean: 

Try the NX CAM Feature-based Machining Starter Kit

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

With the Starter Kit we give NX CAM software users a quick introduction into Feature-based Machining (FBM) with NX CAM.

 

Feature-based machining helps you automatically create machine programs directly from part design models, which reduces programming time by up to 90 percent. NX generates the right machining process using the geometry, and product and manufacturing information (PMI), such as tolerances and surface finish, that is associated with intelligent 3D models.

 

fbm image 1.PNG

 

There are no feature-based machining knowledge requirements to use the kit.  The prerequisites are:  NX CAM knowledge of how to create milling and drilling operations and an understanding of the concept of library tools.  The Starter Kit will come with a predefined example of the machining rules for prismatic and mold & die (ejector plate)  The Starter Kit comes with standard tool library including feeds and speeds.  

 

All NX CAM customers can download the Starter Kit as long as they have a maintenance contract. 

 

You can locate and download the Starter Kit here:  

 

Watch the video to learn more about the NX CAM Feature-based Machining Starter Kit.

 

(view in My Videos)

 

Starter Kit Installation:

Download the FBM Starter Kit

Extract the kit to your local drive.

It is recommended to extract on root directory of your drive. 
i.e. extract the kit to D:\

The kit is separated from your NX installation and doesn’t change your existing NX environment.

 

Starting

README.pdf will explain the Content and where to find what!

Start one of the two Batch Files as introduced inside README.pdf

 

Let us know what you think of the starter kit in the comment section below.

 

fbm image 2.PNGFeature-based Machining Starter Kit

 

 

Comments
Legend
Legend

Good idea Smiley Happy

 

Had to learn it the hard way, though.

Valued Contributor
Valued Contributor

Thank you very much for this starter kit. It is very helpful. 

I have one question... If i would like to change the tooldiameter (like in the video) does i need an additional license to teach the machining roule? 

Thank you 

Best regards 

Dreamer
Dreamer
"Download the Starter Kit here" link destination is invalid..
Pioneer
Pioneer

Hi @Stephanie 

 

I also am unable to download the Starter Kit from the link in the Tech Tip;

 

"The file you specified could not be found"

 

Keith

Community Manager Community Manager
Community Manager

Thank you for informing us that there is a problem with the download page.  I will post notification when the issue is resolved.   Best,  Stephanie