11-06-2016 12:47 PM
Hello,
how can I check if there is a valid license for a robot controller?
I want to prevent, that the user has to click the message box with the missing license multiple times.
11-07-2016 05:39 AM
11-08-2016 03:29 AM
Hello Patrick,
thank you for the hint with the dos shell command.
I will try this possibility for V11.1 soon.
Meanwhile I studied the .Net help files of version 11.1, 12.1.3 and 13.0.2
It seems that in V11 and V12 there are no API functions to check licenses.
But in V13, Tecnomatix has obviously added some classes.
I will also try these new properties, methods and exceptions after I have installed the V13 software.
TxNoLicenseException, MissingLicenseName, ShowMissingLicenseMessage, Licensed are maybe what I am looking for.
Watch Replays of Previous Topics