Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ClonestableID

Genius
Genius

Hallo,

 

I have created an equipment prototype in the PS disconnected, have inserted some devices with the kinematics in the equipment prototype. Now I try to generate XML to import this equipment prototype in project library. For this xml I need CloneStableID for each device in the created equipment prototype.

How can I get this CloneStableID?

1 REPLY

Re: ClonestableID

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Witalij,

 

After creating the equipment prototype, execute End Modeling. This will create the .cojt with all needed information under the system root of your psz.

If the psz is exported from existing eMServer project, then open the project in PS on eMServer and load the psz file.

Then just update the eMServer.

 

Best Regards,

DianaG