Cancel
Showing results for 
Search instead for 
Did you mean: 

Control tx3DVectorCtrl does not have TypeValid and TypeInvalid event

Pioneer
Pioneer

Hi,

 

I added Tx3DVectorCtrl in windows form and applied Picked event. I saw video of "How to add UI" from tecnomatix knowledge base. In that video, TxObjEditBoxCtrl has TypeValid and TypeInvalid events, but Tx3DVectorCtrl does not have these events. I want to get values from Tx3DvectorCtrl after Picked event as well as directly when we write values inside box. How can I do that?

Thanx 

1 REPLY 1
Highlighted

Re: Control tx3DVectorCtrl does not have TypeValid and TypeInvalid event

Legend
Legend

@Bishen 

 

the purposes of the TxObjEditBoxCtrl and Tx3DVectorCtrl are different: first is used to select and object in PS and second is used to edit vector coordinates. Tx3DVectorCtrl just "Resembles three adjacent edit boxes, each with a spinner (up and down arrow buttons). Used to specify a 3D vector. Displays the 3D vector value according to the units set in the Options dialog." The Events TypeValid/TypeInvalid "Occurs when the user enters an valid/invalid object name."