Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating Multiple Part Appearance

Experimenter
Experimenter

Hello everyone,

 

I currently have difficulties trying to create a multiple part appearance from an existing part, relative to an existing location, attaching an existing operation.

 

In the Tecnomatix.Engineering namespace there is a class TxPartAppearance, but it refers to the physical appearance of the part.

 

Is there a method or a class that I didn't find? Or is there no way to call the function "Multiple Part Appearance" as it is and I should create it from scratch (new partappearance, copy the operation, etc...)?

 

Thanks for the help!

 

Francois Neveu

2 REPLIES 2

Re: Creating Multiple Part Appearance

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

Unfortunately, creation a part appearance is not yet exposed in public .NET API.

 

Kind regards,

Zachi

Re: Creating Multiple Part Appearance

Experimenter
Experimenter

That's unfortunate, indeed.

 

Thank you for your quick answer!