Cancel
Showing results for 
Search instead for 
Did you mean: 

Exception for TxFrameComboBoxCtrl

Creator
Creator

Hi,

 

I have a dialog with the Conrol "TxFrameComboBoxCtrl" from the Tecnomatixs Toolbox.

 

When initializing, the value ".... VisualizePickedFrameInGraphicViewer = false;" automatically set.

 

When I run the code, I get the exception:

Method not found: 'Void Tecnomatix.Engineering.Ui.TxFrameComboBoxCtrl.set_VisualizePickedFrameInGraphicViewer (Boolean)'.

 

What do I have to do?

 

Thanks

6 REPLIES 6

Re: Exception for TxFrameComboBoxCtrl

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi SteffiFri,

 

Which version of Tecnomatix is that?

Do you use that control to write a command or a viewer?

 

Best Regards,

DianaG

Highlighted

Re: Exception for TxFrameComboBoxCtrl

Creator
Creator

Hi, 

 
I installed both version 13 (RobotExpert) and version 11 (ProcessSimulate). The toolbox-Items belong to the 13er version.

With a few small tricks the control is now displayed:
  • delete 
    this.txFrameComboBoxCtrl1.VisualizePickedFrameInGraphicViewer = false;
in ...Designer.cs
  • add 
    txFrameComboBoxCtrl1.Size = new System.Drawing.Size(241, 23);
    txFrameComboBoxCtrl1.AutoSize = false;

in Code-Class of the Form

 

Now the Control in displayed, but the picked frame is not displayed!

Re: Exception for TxFrameComboBoxCtrl

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi SteffiFri,

 

If you want to use the code in V11 and V13, then you need to compile it with V11 installation.

VisualizePickedFrameInGraphicViewer property does not exist in V11, it was added in V12.1

 

Best Regards,

DianaG

 

 

 

Re: Exception for TxFrameComboBoxCtrl

Creator
Creator

Is there a Toolbox Dll in V11? I can not find such a file!

Re: Exception for TxFrameComboBoxCtrl

Siemens Phenom Siemens Phenom
Siemens Phenom

eMpower32 folder is not available in V11, you need later version - 12, 13, etc.

But you already have your code designed in V13, so I suggest that you simply compile it with V11 and does not create the project by scratch.

 

Best Regards,

DianaG

Re: Exception for TxFrameComboBoxCtrl

Creator
Creator

Yes, okay that's good to know... I have already thought of something, but I can continue to work in that way!

 

Thanks