Cancel
Showing results for 
Search instead for 
Did you mean: 

Executing simulation runs within a method

Hello

 

I have developed a library in c++ to optimise simulation problems (similar to the GAWizard).

I access the optimisation procedure in the library through a Dialog object I created.

The Dialog object has a method (callback method) which allows for specifying the simulation model parameters such as decision variables and their ranges, as well as the output parameters to be optimised.

 

After I call the library and start the optimisation procedure, I desire to run the simulation problems/models from the library.

When the models are run however, the simulation run is unable to start unless the method calling the library (callback method) execute completely.

I read in the help guide that Tecnomatix Plant Simulation EventController (the object I use to run the models) cannot start or reset a simulation from within a method unless the method fully executes first. So in my case the callback method must fully execute before any simulation run is done in the library, which I do not desire as the optimisation procedure relies on iterative simulation run results.

 

Is there a way around this perhaps? Can't I start (or reset) a simulation run from within a method without fully executing the method?

To summarize, how can I run a TPS model from within a method in a Dialog object while the method is still executing?

 

Thank you in advance,

Simulationist

 

 

2 REPLIES 2
Highlighted

Re: Executing simulation runs within a method

Siemens Legend Siemens Legend
Siemens Legend

Hi.

Are you asking a question regrading the Plant Simulation or Process Simulate? This forum is for the .net API support of Process Simulate only.

 

Re: Executing simulation runs within a method

Hello

It is a question regarding Tecnomatix Plant Simulation.