Cancel
Showing results for 
Search instead for 
Did you mean: 

Export study to .psz file by API

Pioneer
Pioneer

hello,

 

It is possible to export study to .psz file by API ?

 

Regards

3 REPLIES 3

Re: Export study to .psz file by API

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello, Terror_Error,

 

This is possible starting from Tecnomatix V13.1

You can check in the Tecnomatix.NET.chm in the What's New section:

 

Use the LoadDataFromFile or LoadLineSimulationDataFromFile methods of ITxOfflineGlobalServicesProvider to load a psz file in Process Simulate Standalone. To save the changes to a loaded psz file, call to the SaveDataToFile method.
The same functionality is also available on Process Simulate on eMServer platform – refer to the LoadDataFromFile, LoadLineSimulationDataFromFile and SaveDataToFile methods of the ITxEmsGlobalServicesProvider interface.
It is now possible to get the full path of the currently loaded data file (psz, psz-tc or cell) using the FinalDestination property of the TxDocument class.

 

Best Regards,

DianaG

Re: Export study to .psz file by API

Valued Contributor
Valued Contributor
Hello, @DianaG

whether there is a way to insert a .psz file to another .psz file?
or import a .psz file into another study that has open?
then there will be an effective way to merge two studies data.

thanks

Re: Export study to .psz file by API

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi ErnestA,

 

There is a command "Import pszx to Current Study" that imports a study to the current one. To generate a .pszx file use the "Save As" command and choose the relevant "Save as type" from the Save As dialog.

 

Best Regards,

DianaG