Cancel
Showing results for 
Search instead for 
Did you mean: 

Export weld coordinates to excel via API

Experimenter
Experimenter

Hello,

 

I want to develop a tool for process simulate that exports the coordinates of weld locations in a given operation to excel. I also want them in relashionship to the self origin of the part they belong to, but this can be implemented later.

 

My question is: is this possible with the API? Do we have any sample code or directions I could take to begin with it.

 

Thank you Smiley Happy

1 REPLY 1

Betreff: Export weld coordinates to excel via API

Legend
Legend

Hi,

yes it can be done via API.

Iterate through the operation. If location is of type TxWeldLocationOperation then export coordinates stored in AbsoluteLocation-Property.

It is not very difficult!