Cancel
Showing results for 
Search instead for 
Did you mean: 

How can you develop the program conveniently?

Pioneer
Pioneer

Hi Experts:

    i begin to develop the Tecnomatix Software  using C# recently.I've learned how to create commands on the toolbar by watching videos on my website. But what else can I do instead of creating command buttons to execute my program? In addition, can tecnomatix software obtain objects through external programs? For example, an external program obtains a tecnomatix object by such a method: GetObject ("Tecnomatix.Application"), and I can get the object inside without closing the software. Because I feel the create command, the command register development means, develop special trouble, whenever I modify the program, need to recompile and restart tecnomatix software, frequent closed and open software costs time and effort.Or is there a method that does not need to shut down tecnomatix after each revision, and can be used directly in tecnomatix after re generation.

    I am a novice, I hope the master can teach some skills.

6 REPLIES 6

Re: How can you develop the program conveniently?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

There is no need to close PS, recompile and restart PS.

You can start PS directly from Visual Studio into Debugging mode.

So you can set breakpoints in VS and the debugger will stop at this points, in addition you can pause the debugger, modify your code and play with the modified code.

 

Therfore, setup your project properties in VS.

The example shows the arguments for PS Disconnected. If you want to use for eMS Based use
"/c NewAssembler /l ems"

As an output path of your dll file set the "TecnomatixDir\eMPower\DotNetCommands".

E.g. 

debug.png

 

Best regards

Patrick

Re: How can you develop the program conveniently?

Pioneer
Pioneer

 thank you PatrickUnangst,it's so cool!It's too convenient!

 

Re: How can you develop the program conveniently?

Legend
Legend

Additionally you can use /command command line option to start specific command automatically.

Re: How can you develop the program conveniently?

Pioneer
Pioneer

thank you ,but can you give me a few  examples?

Re: How can you develop the program conveniently?

Legend
Legend

Take a look hier: Open project on eMServer from command line last comment from DianaG.

Re: How can you develop the program conveniently?

Legend
Legend

What I am really missing is the possibility to test programs with unit tests and so on. This make the development process much more unsafe and expensive.