Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add Resource Library?

Valued Contributor
Valued Contributor

I have looked at

TxApplication.CommandsManager.ExecuteCommand("EMServer.New");

 

which is really not any different than just doing it manually.  From what I can tell, unfortunately, this command does not appear to take a parameter so it still requires user input to tell what you want to add (PmResourceLibrary, PmToolPrototype).

 

txNewPartResourceParametersEx.Type = "PmResourceLibrary";
TxApplication.CommandsManager.ExecuteCommand("ComponentOperations.NewResource", txNewPartResourceParametersEx);

This performs how I would like, creating the Resource Library without user input, however, it creates it in the object tree, not the library.

 

 

Is there a way to do this, but adding this to the library?

 

Also, as a side note, I see that there are "EMServer.CheckIn" and "EMServer.CheckOut" commands, but I haven't found a IsCheckedIn or IsCheckedOut property for anything.  So I'm wondering how do I test if something is checked out (in) before I check it out (in)?

7 REPLIES 7

Re: How to add Resource Library?

Valued Contributor
Valued Contributor

For the second question, I did find TxEmsServicesProvider, which has CheckInCheckOutState

Re: How to add Resource Library?

Legend
Legend

The first task is much easier to achieve with eM Server API.

Highlighted

Re: How to add Resource Library?

Valued Contributor
Valued Contributor

Is there any documentation for the eM Server API?  I only see Tecnomatix.NET.chm for SDK help.

Re: How to add Resource Library?

Legend
Legend

Sorry, for the delay. I have got eM-PlannerAPIManual .chm file from our system administrator, usually it is a part of the installation.

Best Regards,

witalij.

Re: How to add Resource Library?

Siemens Legend Siemens Legend
Siemens Legend

Hi,

it should be on the istallation disk- under the Documentation folder.

Re: How to add Resource Library?

Valued Contributor
Valued Contributor

Thanks, I am having our IT department look into it. 

 

Out of curiosity, is this part of the Process Sim installation or is there a seperate installation just for emServer?

Re: How to add Resource Library?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

It is available in the Documentation folder of the Setup CD. As far as I know, it is not copied to the setup folder of Process Simulate.

 

Best Regards,

DianaG